DOCA0157EN-09

Status Monitoring and Load Control

PowerTag Control IO 230 V Module

Load control with feedback loop can be achieved with PowerTag control IO 230 V module (reference A9XMC1D3).

WARNING
UNEXPECTED START OF OPERATION
Only use PowerTag control IO 230 V module (reference A9XMC1D3) and PowerTag control 2DI 230 V module (reference A9XMC2D3) to control electrical loads that can be safely left unattended.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: It is not possible to use the input of the PowerTag control IO module as an independent input from the control circuit of the output. This input is dependent on the output and used as backloop.

With this solution, it is possible to easily control remotely a contactor (CT) or an impulse relay (TL) with or without the information of the load circuit contact using the associated input.

Local Output Control

During the commissioning phase, you will select whether the output order should be a pulse (for impulse relay) or a latch order (for contactor). Once the IO module has been commissioned, the front face push button allows to change the status of output control circuit.

Commissioning and decommissioning are done through webpages.

NOTE: The push button is not active when the LED is yellow or Off.

The push button can also be used for decommissioning in case of communication loss (>240 s)

To commission or decommission the PowerTag control IO 230 V module, refer to Wireless Device Commissioning with Webpages or refer to EcoStruxure Power Commission Online Help.

To configure the PowerTag control IO 230 V module, refer to the following procedure or EcoStruxure Power Commission Online Help.

Step

Action

1

Click Start Scanning to discover the wireless devices connected to the PowerTag Link gateway.

Result: Displays the discovered wireless devices and assigns Modbus address to each device.

2

Select any wireless device and click the pencil icon to modify the configuration of the selected wireless device.

3

Enter the Asset Name of a wireless device.

4

Enter the Label of a wireless device.

5

Enter the Usage from the drop-down list.

6

Enter the Configuration Type from the drop-down list.

7

Enter the Output Contact type from the drop-down list.

8

Check the Feedback Loop box if necessary.

9

Enter the Feedback Loop Contact type from the drop-down list.

10

If necessary, enable the Local Control by ticking the associated box.

11

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.