DOCA0157EN-09

Alarms Output Table

Alarms Output

Alarm description

Wireless device

Alarm output

PowerTag Energy sensors

PowerTag control modules

HeatTag sensor

Modbus register

Email notifications

 

PowerTag Link display

Generic

Specific

Communication loss

ü

ü

ü

ü

ü

   

Voltage loss

ü

   

ü

ü

 

ü

Overcurrent at voltage loss

ü

   

ü

ü

 

ü

80% of nominal current

ü

     

ü

   

50% of nominal current

ü

     

ü

   

45% of nominal current

ü

   

ü

     

Zero current

ü

   

ü

     

Undervoltage (80%)

ü

   

ü

     

Overvoltage (120%)

ü

   

ü

     

Partial active energy delivered

ü

       

ü

 

Partial active energy received

ü

       

ü

 

Current I

ü

       

ü

 

Voltage phase-to-neutral

ü

       

ü

 

Voltage phase-to-phase

ü

       

ü

 

Total active power

ü

       

ü

 

Phase active power

ü

       

ü

 

Power factor

ü

       

ü

 

Load operating time counter

ü

       

ü

 

Digital input switch

 

ü

     

ü

ü(1)

Temperature 

   

ü

   

ü

ü(1)

Relative humidity 

   

ü

   

ü

ü(1)

HeatTag alarm

   

ü

ü

     

Preventive maintenance on device

   

ü

ü

     

Device replacement

   

ü

ü

     
(1) The alarm is displayed on the PowerTag Link display, only if specific alarm is configured in the PowerTag Link gateway.
NOTE: It is possible to create up to 25 additional specific email notifications. These notifications are sent based on measures or status analysis. For example, Alarm trip for PowerTag control 2DI module.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.