DOCA0157EN-09

Backup Generation

After finishing the commissioning, it is highly recommended to back up the configuration. This will save information that are mandatory in case of replacement of the PowerTag Link gateway.

If the back up is not done, and if the PowerTag Link gateway is malfunctioning or inoperative and needs to be replaced, then all sensors which are connected to the PowerTag Link gateway should be replaced or unpaired. This will lead to:

  • Over cost (for the installation of the replacement sensors)

  • Shut down of the switchboard to access the sensor

Follow the steps given in the table to generate the Backup file:

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Maintenance > Backup & Restore.

4

Click Backup button to generate the file.

Result: The backup file with name backup.dat will be automatically saved on your PC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.