DOCA0157EN-09

Identification

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > General > Identification.

The Identification page is used to edit the gateway name and it displays the following parameters:

Parameters

Description

Gateway Identification

User Application Name

You can customize the name of the gateway used by communication services.

Product Range

Displays the product range name of the gateway.

Product Model

Displays the product model name of the gateway.

Serial Number

Displays the serial number of the gateway.

Firmware Revision

Displays the firmware version number of the gateway.

Unique identifier

Displays the identifier used by communication protocols.

Webpage Version

Displays the webpage version of the gateway.

Building Information

Building Name

You can customize the name of the gateway place inside the building.

The Device Name is same as the name displayed in Windows Explorer.

NOTE: The Device Name should contain only alphanumeric characters and a hyphen (-) character. The ‘-’ character cannot be the last character.

Click Apply Changes to save the changes. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.