DOCA0157EN-09

Status Monitoring

PowerTag Control 2DI 230 V Module

Status monitoring alone is achieved with PowerTag control 2DI 230 V module (reference A9XMC2D3).

With this solution, you can easily know the status of two contacts or achieve OF/SD daisy chain.

Commissioning and decommissioning are done through webpages.

NOTE: In case of communication loss, the push button is used for decommissioning (>240 s).

To commission or decommission the PowerTag control 2DI 230 V module, refer to Wireless Device Commissioning with Webpages or refer to EcoStruxure Power Commission Online Help.

To configure the PowerTag control 2DI 230 V module, refer to the following procedure or EcoStruxure Power Commission Online Help.

Step

Action

1

Click Start Scanning to discover the wireless devices connected to the PowerTag Link gateway.

Result: Displays the discovered wireless devices and assigns Modbus address to each device.

2

Select any wireless device and click the pencil icon to modify the configuration of the selected wireless device.

3

Enter the Asset Name of the Input 1.

4

Enter the Label of the Input 1.

5

Select the Usage from the drop-down list.

6

Select the Configuration Type from the drop-down list.

7

Select the Contact type from the drop-down list.

8

Repeat these actions for the Input 2.

9

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.