DOCA0157EN-09

Load Monitoring Modbus Registers

Description

The Modbus registers of the wireless device allows you to monitor the following status in any supervision system:

  • Alarm with two types:

    • The voltage loss of the load.

    • If an overload has occurred at the voltage loss event.

  • Load Operating Time: The duration of how long the load worked effectively (above a certain power, this avoiding idle/standby times to be counted), to optimize the maintenance times.

Applicable Devices

The code in the Applicable Devices column indicates the types of wireless device for which the register is available:

  • A: the register is available for PowerTag Energy ●63 (A9MEM152●, A9MEM154●, A9MEM156●, and A9MEM157●)

  • M: the register is available for PowerTag Energy M250/M630 (LV43402●)

  • R: the register is available for PowerTag Energy F160 (A9MEM1580) and Rope (A9MEM159●)

Alarm

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x0CE1

3298

1

R

BITMAP

0xFFFF

N

03,

100–4

A/M/R

Validity of the alarm bitmap (register 3300)

  • 0 = Invalid.

  • 1 = Valid.

0x0CE2

3299

1

Reserved

0x0CE3

3300

1

R

BITMAP

0xFFFF

N

03,

100–4

A/M/R

Alarms bitmap

0 = Alarm OFF.

1 = Alarm ON.

Bit 0 = Voltage loss

Bit 1 = Current overload at voltage loss

Bit 2 = Reserved

Bit 3 = Overload 45%

Bit 4 = Load current loss

Bit 5 = Overvoltage 120%

Bit 6 = Undervoltage 80%

Bit 7 = Battery low

0x0CE4

3301

1

Reserved

0x0CE5

3302

2

R

NA

A

Float32

NA

0xFFC00000

N

03,

100–4

A/M/R

RMS current on phase A at voltage loss (last RMS current measured when voltage loss occurred)

0x0CE7

3304

2

R

NA

A

Float32

NA

0xFFC00000

N

03,

100–4

A/M/R

RMS current on phase B at voltage loss (last RMS current measured when voltage loss occurred)

0x0CE9

3306

2

R

NA

A

Float32

NA

0xFFC00000

N

03,

100–4

A/M/R

RMS current on phase C at voltage loss (last RMS current measured when voltage loss occurred)

Load Operating Time

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x0CEB

3308

2

RW

s

UINT32

0xFFFFFFFF

Y

03,

100–4

A/M/R

Load operating time counter.

0x0CED

3310

2

RW

W

Float32

0xFFC00000

Y

03,

100–4

A/M/R

Active power threshold for Load operating time counter. Counter starts above the threshold value.

0x0CEF

3312

4

RW

DATETIME

0x00000000

Y

03,

100–4

A/M/R

Date and time stamp of last Set or reset of Load operating time counter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.