DOCA0157EN-09

Alarm Configuration for PowerTag Control Module

Follow the steps given in the table to setup an alarm for PowerTag control module:

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > Alarms > Alarm Configuration.

4

Click Add Alarm.

5

Select Specific Alarms.

6

Select Asset Name as PowerTag control.

7

Set the alarm conditions depending on when you want to trigger the alarm.

For example, when the Digital Input is On To Off or when Digital Input is Off To On.

8

Select the required email address from the ...Then Send E-mail to to send the notification in case of an alarm.

9

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.