DOCA0157EN-09

PowerTag Link Gateway

PowerTag Link Gateway Acting as a Concentrator

The wireless communication devices provide compact and high density metering and monitoring solution with rich and accurate data for building systems (that can send energy, power, current, voltage, temperature, and power factor to PowerTag Link gateway).

Description

A
Power supply connector 110-230 Vac
B
Default IPv4 address
C
Communication status indicators
  • Status LED

  • LK/10-100/ACT LED

  • Wireless LED

D
Reset button
E
RJ45 Ethernet connection

For more information on installation, refer to PHA81113 PowerTag Link Gateway – Instruction Sheet.

Status LED

Operating Mode

Status LED

Status

Initialization / Operation

Green light: The gateway operates normally.

Start-up

Alternate green and red light every second: The gateway is starting.

Factory settings

Orange light: The gateway

  • is in DHCP client mode, or

  • DHCP server has not assigned IP address

Reset (level 1)

Green blink: While pressing the Reset button between 5 and 10 seconds, IP settings are reconfigured to DHCP mode.

Reset (level 2)

Red blink (Fast, 2 blinks/sec): While pressing the Reset button for more than 10 seconds, the LED stops blinking after the Reset button is released. Do not switch off the gateway until the LED stops blinking in red for at least 30 seconds, as the reset level 2 is still in progress.

Duplicate IP address

Red blink (1 blink per second): The gateway has detected duplicate IP address. Check and change the IP address of the gateway.

Degraded

Orange blink: Power supply of the gateway is degraded.

Failure

Red light: The gateway is out of order.

LK/10-100/ACT LED

LK/10-100/ACT LED

Status

Orange blink: Ethernet activity at 10 Mbps

Green blink: Ethernet activity at 100 Mbps

Wireless LED

Operating Mode

Wireless LED

Status

Initialization

Orange light: Not configured

Start-up

Orange blink: Looking for wireless device

Operation

Flash green every five seconds: Networking complete (normal operation)

Degraded

Green blink (1 blink per 5 seconds): Downgraded while boot mode

Disabled

Light off: Wireless disabled

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.