DOCA0157EN-09

Overview

The commissioning of a PowerTag Link gateway can be performed using:

  • the EcoStruxure Power Commission (EPC) software. Refer to EcoStruxure Power Commission Online Help.

  • the PowerTag Link webpages. The webpages are autonomous to configure any devices connected or paired with PowerTag Link gateway.

NOTE:
  • Before commissioning the PowerTag Link gateway, upgrade the firmware of the PowerTag Link gateway.

  • The firmware upgrade of the PowerTag Link gateway can only be done using the EcoStruxure Power Commission software. Refer to EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.