DOCA0157EN-09

Restore Operation

It is possible to replace a malfunctioning or inoperative PowerTag Link gateway with a new one, and to restore the setup if the backup file has been previously generated at the end of the commissioning process.

Follow the steps given in the table to restore and configure the setup:

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Maintenance > Backup & Restore.

4

Click Browse to select the backup file.

5

Click Backup button to restore the configuration.

  • Validate the restore operation in the confirmation pop-up window and click Yes.

  • Wait till the end of the restoration process.

NOTE: The Backup and Restore function works only for the same PowerTag Link gateway reference. It means that you can only apply a backup file from a A9XWD20 to a A9XWD20 and not from a A9XMWD20 to a A9XMWD100.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.