DOCA0157EN-09

Partial Active Energy Delivered

This alarm indicates that the Partial Active Energy Delivered has reached the configured threshold value. The alarm can be set with the following conditions:

  • Greater than: The alarm is triggered when the Partial Active Energy Delivered exceeds the configured threshold value.

  • Every: The alarm is triggered every time the Partial Active Energy Delivered has reached the time configured in the threshold value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.