DOCA0157EN-09

PowerTag Control Modules Modbus Registers

Digital Input 1 Registers

The following table provides the registers that are available for PowerTag control IO and PowerTag control 2DI modules.

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Description

0x84D0

34001

10

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital input 1 name

0x84DA

34011

13

Reserved

0x84E7

34024

3

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital input 1 circuit identifier

0x84EA

34027

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 product usage(1)

0x84EB

34028

1

Reserved

0x84EC

34029

1

R

NA

NA

UINT16

NA

0x8000

Y

03,

100-4

Digital input 1 assignment reference(2)

When digital output 1 feedback loop is configured to 'Enabled', the register is forced to 'Feedback loop' (16), (see register 37036, refer to Digital Output 1 Registers).

0x84ED

34030

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 contact type

  • 0 = Normally open

  • 1 = Normally close

0x84EE

34031

10

Reserved

0x84F8

34041

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 electrical status

Indicates the electrical status of the input regardless of the assignment reference

  • 0 = Low level

  • 1 = High level

0x84F9

34042

5

Reserved

0x84FE

34047

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 breaker position

Indicates the breaker position – Only available if input 1 assignment reference is 'Breaker position' (case = 2)

  • 0 = Open

  • 1 = Close

0x84FF

34048

9

Reserved

0x8508

34057

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 trip indicator

Indicates the trip status – Only available if input 1 assignment reference is one of the trip causes (case = 3 to 8)

  • 0 = Tripped

  • 1 = Not tripped

0x8509

34058

7

Reserved

0x8510

34065

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 1 status

Indicates the status of the digital input 1 – Only available if input 1 assignment reference is not 'Breaker position' or none of the trip causes (Cases 1, 9, 15, 16)

  • 0 = On

  • 1 = Off

(1) For the register 34027, the various Digital input 1 product usage are:

  • 1 = Main/Incomer

  • 2 = Sub/Head of group

  • 3 = Heating

  • 4 = Cooling

  • 5 = HVAC

  • 6 = Ventilation

  • 7 = Lighting

  • 8 = Office Equipment

  • 9 = Cooking

  • 10 = Food refrigeration

  • 11 = Elevators

  • 12 = Computers

  • 13 = Renewable Energy Production

  • 14 = Genset

  • 15 = Compressed air

  • 16 = Vapor

  • 17 = Machine

  • 18 = Process

  • 19 = Water

  • 20 = Other sockets

  • 21 = Other

(2) For the register 34029, the various Digital input 1 assignment reference are:

  • 0 = None

  • 1 = Standard input

  • 2 = Breaker position

  • 3 = Trip indicator (SD)

  • 4 = Chained trip indicator

  • 5 = Electrical trip signal contact

  • 6 = Thermal trip signal contact

  • 7 = Earth leakage trip signal contact (SDV)

  • 8 = Groud fault trip signal contact

  • 9 = Surge failure contact

  • 15 = Switchboard board door contact

  • 16 = Feedback loop

NOTE: For the registers 34041, 34047, 34057, and 34065, the value of the configuration is normally open. If the register 34030 is normally close, then switch the description of the registers 34041, 34047, 34057, and 34065. So, basically for these registers, 0 becomes 1 and 1 becomes 0, when they are normally close.

Digital Input 2 Registers

The following table provides the registers that are available for PowerTag control 2DI module only.

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Description

0x8534

34101

10

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital input 2 name

0x853E

34111

13

Reserved

0x854B

34124

3

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital input 2 circuit identifier

0x854E

34127

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 product usage(1)

0x854F

34128

1

Reserved

0x8550

34129

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 assignment reference(2)

0x8551

34130

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 contact type

  • 0 = Normally open

  • 1 = Normally close

0x8552

34131

10

Reserved

0x855C

34141

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 electrical status

Indicates the electrical status of the input regardless of the assignment reference

  • 0 = Low level

  • 1 = High level

0x855D

34142

5

Reserved

0x8562

34147

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 breaker position

Indicates the breaker position – Only available if input 2 assignment reference is in 'Breaker position' (case = 2)

  • 0 = Open

  • 1 = Close

0x8563

34148

9

Reserved

0x856C

34157

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 trip indicator

Indicates the trip status – Only available if input 2 assignment reference is one of the trip cause (case = 3 to 8)

  • 0 = Tripped

  • 1 = Not tripped

0x857D

34158

7

Reserved

0x8574

34165

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital input 2 status

Indicates the status of the digital input 2 – Only available if input 2 assignment reference is not 'Breaker position' or none of the trip causes (Cases 1, 9, 15, 16)

  • 0 = On

  • 1 = Off

(1) For the register 34127, the various Digital input 2 product usage are:

  • 1 = Main/Incomer

  • 2 = Sub/Head of group

  • 3 = Heating

  • 4 = Cooling

  • 5 = HVAC

  • 6 = Ventilation

  • 7 = Lighting

  • 8 = Office Equipment

  • 9 = Cooking

  • 10 = Food refrigeration

  • 11 = Elevators

  • 12 = Computers

  • 13 = Renewable Energy Production

  • 14 = Genset

  • 15 = Compressed air

  • 16 = Vapor

  • 17 = Machine

  • 18 = Process

  • 19 = Water

  • 20 = Other sockets

  • 21 = Other

(2) For the register 34129, the various Digital input 2 assignment reference are:

  • 0 = None

  • 1 = Standard input

  • 2 = Breaker position

  • 3 = Trip indicator (SD)

  • 4 = Chained trip indicator

  • 5 = Electrical trip signal contact

  • 6 = Thermal trip signal contact

  • 7 = Earth leakage trip signal contact (SDV)

  • 8 = Groud fault trip signal contact

  • 9 = Surge failure contact

  • 15 = Switchboard door contact

  • 16 = Feedback loop

Digital Output 1 Registers

The following table provides the registers that are available for PowerTag control IO module only.

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Description

0x9088

37001

10

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital output 1 name

0x9092

37011

13

Reserved

0x909F

37024

3

R

NA

NA

ASCII

NA

0x00

Y

03,

100-4

Digital output 1 circuit identifier

0x90A2

37027

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital output 1 product usage(1)

0x90A3

37028

1

Reserved

0x90A4

37029

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital output 1 behavior

  • 0 = Normal

  • 1 = Latched

0x90A5

37030

2

Reserved

0x90A7

37032

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital output 1 contact type

  • 0 = Normally open

  • 1 = Normally close

0x90A8

37033

1

Reserved

0x90A9

37034

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital output 1 local control enable

  • 0 = Disable

  • 1 = Enabled

0x90AA

37035

1

Reserved

0x90AB

37036

1

R

NA

NA

UINT16

NA

0xFFFF

Y

03,

100-4

Digital output 1 feedback loop enable.

When output is configured to 'Latched' behavior, register is forced to 'enabled' (see register 37029). When the register is enabled, feedback data are available in Input 1 registers (starting from register 34001).

  • 0 = Disable

  • 1 = Enabled

0x90AC

37037

14

Reserved

0x90BA

37051

1

RW

NA

NA

UINT16

NA

0xFFFF

N

03, 06, 16,

100-4

Digital output 1 command

NOTE: Off and On commands (value 1 and 2) are possible only if the control device is a PowerTag control IO module with configuration type set to ‘contactor’
  • 0 = No command

  • 1 = Off command

  • 2 = On command

  • 3 = Toggle command

0x90BB

37052

1

R

NA

NA

UINT16

NA

0xFFFF

N

03,

100-4

Digital output 1 status

Only significant if output is configured to 'Normal' behavior. (see register 37029). Otherwise, the output is set to invalid value.

  • 0 = Off

  • 1 = On

(1) For the register 37027, the various Digital output 1 product usage are:

  • 1 = Main/Incomer

  • 2 = Sub/Head of group

  • 3 = Heating

  • 4 = Cooling

  • 5 = HVAC

  • 6 = Ventilation

  • 7 = Lighting

  • 8 = Office Equipment

  • 9 = Cooking

  • 10 = Food refrigeration

  • 11 = Elevators

  • 12 = Computers

  • 13 = Renewable Energy Production

  • 14 = Genset

  • 15 = Compressed air

  • 16 = Vapor

  • 17 = Machine

  • 18 = Process

  • 19 = Water

  • 20 = Other sockets

  • 21 = Other

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.