DOCA0157EN-09

Overview

Inoperative gateway replacement is a feature that allows you to download the configuration of the gateway. If the gateway breaks down, you can upload the old configuration that was saved in the new gateway.

NOTICE
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Encrypt the file and protect it with a password to make sure that the configuration file integrity and confidentiality is preserved. Most compression utilities can perform such an operation.
  • Store the encrypted archive in a location on a PC or a network directory where access controls are enforced to prevent any unauthorized access to the file.
Failure to follow these instructions can result in equipment damage.
NOTE: The configuration file generated by the PowerTag Link gateway contains sensitive information about the security of the PowerTag Link gateway.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.