DOCA0157EN-09

HeatTag Sensor

Overview

The HeatTag sensor is a wireless sensor for early detection of overheating wire connections or overheating cables.

The HeatTag sensor helps to prevent electrical distribution switchboards from being damaged by analyzing gas and micro-particles in the air of the switchboard and sending alerts before any smoke or insulator browning.

Features

The HeatTag sensor includes the following features:

  • 3 levels of alert according to the criticality of the detected situation

  • 11 levels of air quality index (0 to 10)

  • Analysis of gas and micro-particles emitted by cable sheaths when overheating

  • Measurement of temperature and humidity in the switchboard

  • Self-diagnostics

  • Communication with PowerTag Link gateway

  • Integration in EcoStruxure™ solutions

For more information on the HeatTag sensor, refer to DOCA0171EN HeatTagWireless Sensor for Early Detection of Overheating Cables – User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.