DOCA0157EN-09

Overvoltage (120%)

This alarms triggers when a phase-to-neutral voltage or a phase-to-phase voltage exceeds the threshold of 120% of the nominal value. The alarm automatically disappears when the voltage remains lower than 108% of the nominal value (a hysteresis of 10% is applied).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.