DOCA0157EN-09

Modbus Synthesis Tables

Description

The Modbus synthesis table provides a synthesis of information from all the wireless devices at a time. By default, the synthesis table is based on Modbus address 247.

NOTE: The synthesis table address is the first one available in decreasing order from 247.

Applicable Devices

The code in the Applicable Devices column indicates the types of wireless devices for which the register is available:

  • A: the register is available for PowerTag Energy ●63 (A9MEM152●, A9MEM154●, A9MEM156●, and A9MEM157●)

  • M: the register is available for PowerTag Energy M250/M630 (LV43402●)

  • R: the register is available for PowerTag Energy F160 (A9MEM1580) and Rope (A9MEM159●)

  • IO: the register is available for PowerTag control IO module (A9XMC1D3)

  • 2DI: the register is available for PowerTag control 2DI module (A9XMC2D3)

  • D: the register is available for PowerTag Link display (A9XMWRD)

  • H: the register is available for HeatTag sensor (SMT10020)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.