DOCA0157EN-09

Settings

The Email Service page is used to configure the email server settings.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > Communication > Email Service.

Click the Enable check box to configure the email server settings (enabled by default). The PowerTag Link gateway allows you to define your own SMTP server.

Follow the steps given in the table to configure the email server settings:

Step

Action

1

Enter the email server name or IP address in the SMTP Server Address area.

2

Select the type of security mode from the Connection Security Mode list.

The following are the available connection security modes:

  • None

  • TLS/SSL

  • STARTTLS

3

Enter the server port value in the SMTP Server Port area. The value ranges from 1 to 65535.

4

Select Authentication if the server requires login information. This option is disabled by default.

5

Enter the user name in the SMTP Account Login area.

6

Enter the password to authenticate the SMTP login in the SMTP Account Password area.

7

Enter the email address of the administrator who is administering the gateway in the From Address area.

The From Address can be used in different ways:

  • Use the From Address as a context provider: If you want to notify and does not want to receive a reply, use a From Address as contextual information. The From Address syntax includes “no-reply”, “gateway name”, “site name”, @a validated domain .com, .net, and so on.

  • Create an alias in the From Address to allow replies to be sent to the person in charge of an alarm: An email can be sent to multiple people who are responsible for a specific appliance. This feature allows the receivers to reply to follow up with the responsible person.

    For example, if the facility manager receives an email from an alarm, the facility manager can send a reply email to the Maintenance Contractor to follow up on the action.

8

Select the language of the email body from the Language list: French or English.

9

Click Apply Changes to save the settings. If you do not want to save the changes, click Cancel Changes.

10

Enter the email address of the recipient to test the delivery of the email in the Recipient Address for Test area.

The test email feature enables connection from the gateway to the service. If the test emails are not received, the Internet connection needs to enable the email ports (port 25 or 587). The port settings are configured in accordance between the gateway that sends the email and the site router settings.

11

Click Test to deliver the email to the added recipient.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.