DOCA0157EN-09

Communication Loss

This alarm indicates that the gateway has lost the communication with a wireless device.

The communication loss happens if the gateway has not received packets for a period of time equal to 6 times the communication period of the device.

The alarm will automatically disappear as soon as the wireless device is connected to the RF network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.