DOCA0157EN-09

Configuration Procedure of HeatTag Sensors with Webpage

Step

Action

1

Navigate to Settings > Devices > Wireless Devices to view the list of the paired wireless devices. For more information on discovering the wireless devices, refer to Pairing Principle.

Result: A list of paired devices is displayed.

2

Select the required HeatTag sensor and click the pencil icon to modify the configuration of the selected wireless device.

Result: The parameters of the HeatTag sensor are displayed.

3

Enter the Modbus Address.

4

Enter the Asset Name of the wireless device.

5

Enter the Label of the wireless device.

6

Select the Equipment to define in which environment the HeatTag sensor is mounted.

7

Select the Sensor position to choose in which position the HeatTag sensor is mounted.

8

Enter the Cubicle Id to define in which cubicle the HeatTag sensor is installed.

NOTE: The value of Cubicle Id ranges between 1 and 20.

9

Select the Cubicle Type to define the cubicle configuration.

NOTE: The options displayed for Cubicle Type depends on the sensor position selected.

10

Enter the Drawer Id to define in which drawer the HeatTag sensor is installed.

NOTE: This option is available only if the Sensor position is selected as LV Drawer. The value of Drawer Id ranges between 1 and 10.

11

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

NOTE: The above settings are available only for LV Switchboard.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.