DOCA0157EN-09

Unpairing of Wireless Devices with Webpage

To unpair a wireless device using the PowerTag Link webpage, follow the steps in the subsequent sections, as applicable.

Some wireless devices have a local method to unpair the devices. Refer to the instruction sheet of the specific device.

IMPORTANT: When unpairing unpowered wireless devices from the PowerTag Link gateway, the devices are removed from the gateway settings, but, for each of these devices, a reference to the gateway remains stored in the device. To pair the wireless device with a new PowerTag Link gateway, perform a local reset to factory settings of the device: power off the device then the device turns to gateway search mode.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.