DOCA0157EN-09

Communication Diagnostic

Wireless Discovered Devices – 100 Devices

Address

Register

No

RW

X

Unit

Type

Range

Invalid value

Svd

Function Code

Applicable Devices

Description

0x9C40

40001

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Validity of the alarm communication status  of the 1st device (register 40002)

  • 0 = Invalid

  • 1 = Valid

0x9C41

40002

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Communication status between the PowerTag Link gateway and the 1st device

  • 0 = Communication loss

  • 1 = Communication OK

0x9C42

40003

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Validity of the alarm communication status  of the 2nd device (register 40004)

  • 0 = Invalid

  • 1 = Valid

0x9C43

40004

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Communication status between the PowerTag Link gateway and the 2nd device

  • 0 = Communication loss

  • 1 = Communication OK

...

...

...

...

...

...

...

...

...

...

...

...

...

0x9D06

40199

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Validity of the alarm communication status  of the 100th device (register 40200)

  • 0 = Invalid

  • 1 = Valid

0x9D07

40200

1

R

NA

NA

BITMAP

NA

0x0000

N

 03,

100–4

A/M/R

IO/2DI

D/H

Communication status between the PowerTag Link gateway and the 100th device

  • 0 = Communication loss

  • 1 = Communication OK

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.