DOCA0157EN-09

Time Zone

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > General > Time Zone.

The Time Zone page is used to configure the offset and daylight saving time for the selected time zone.

Follow the procedure to configure the time zone settings:

Step

Action

1

Click the offset value used by the local time zone from the Time Zone Offset list.

2

Select the Enable check box to configure the daylight time saving settings. The Enable check box is not selected by default.

3

Select the day, month, and time to configure the start time of daylight saving time from the respective Daylight Saving Time Begins list.

4

Select the day, month, and time to configure the end time of daylight saving time from the Daylight Saving Time Ends list.

5

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.