DOCA0157EN-09

Active Power Demand

Power Demand

PowerTag Link/PowerTag Link HD gateway provides:

  • Total active power demand calculated on a sliding block interval.

  • Maximum of the total active power demand.

  • Date and time of occurrence of that maximum.

Power Demand Calculation

Power demand is calculated using arithmetical integration of the power value during a period of time (interval) divided by the length of the interval. The result is equivalent to the energy accumulated during the interval divided by the length of the interval.

Interval for Power Demand Calculation

Power demand is calculated over a sliding block interval. Navigate to Settings > Devices > Global Configuration to set the interval duration from 1 to 60 minutes. The default value is 10 minutes.

Maximum Power Demand

The maximum power demand is the highest value calculated since the beginning of the measurement or the last reset. The PowerTag Link/PowerTag Link HD gateway time stamps (date and time) the maximum power demand occurrence.

The PowerTag Link/PowerTag Link HD gateway stores the maximum power demand and the associated date and time.

Resetting the Maximum Power Demand

  1. Navigate to Settings > Devices > Global Configuration

  2. Click Reset all Max Demands to reset the maximum power demand.

Once the reset is done, the below message appears on the screen.

NOTE: The active power demand is only available for the PowerTag Energy sensors with firmware version 003.000.386 or later.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.