DOCA0157EN-09

Wireless Communication Devices

Description

Wireless communication devices that can be connected to the PowerTag Link gateway are:

  • A9MEM152● or A9MEM154●, PowerTag Energy M63

  • A9MEM156● or A9MEM157●, PowerTag Energy F63 and P63

  • A9MEM1580, PowerTag Energy F160

  • A9MEM159●, PowerTag Energy Rope

  • LV43402●, PowerTag Energy M250/M630

  • A9XMC●D3, PowerTag control modules

  • SMT10020, HeatTag sensor

  • A9XMWRD, PowerTag Link display

For more information on wireless communication devices, refer to CA908058E PowerTag Energy – Selection Guide.

Principle of Wireless Device Installation

The PowerTag Link gateway is installed in such a manner that the wireless communication devices are distributed around the gateway. It is recommended to install the PowerTag Link gateway in the center of the switchboard. The distance between the wireless communication devices and the gateway should be less than 3 meters for installing in simple plastic panels (for example, Kaedra panel) up to multi-columns (non-partitioned, form 2) metallic switchboard (for example, PrismaSet panel).

NOTE: There is a possibility of disruption in the quality of radio frequency signal if wireless communication devices are installed in a different switchboard (particularly if the enclosure has metallic partitions and door).

For more information on wireless device installation, refer to DOCA0194EN PowerTag System – Design and Commissioning Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.