DOCA0157EN-09

Undervoltage (80%)

This alarms triggers when a phase-to-neutral voltage or a phase-to-phase voltage falls below the threshold of 80% of the nominal value. The alarm automatically disappears when the voltage remains greater than 88% of the nominal value (a hysteresis of 10% is applied).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.