9065CT9701R03/21

Application

Hand reset melting alloy overload relays use a eutectic alloy solder, which responds to the heat produced in a heater element by the motor current. When tripped, the overload relay can be reset manually after allowing a few minutes for the motor and overload relay to cool and the solder to solidify.

Schneider Electric one-piece thermal unit construction provides overload protection for the majority of motors. Repeated tripping does not affect the original calibration. Melting alloy thermal units are available in three designs:

  • Standard Trip (Class 20): All standard trip thermal units provide trip characteristics for normal motor acceleration up to approximately 7 seconds on a full voltage start.

  • Slow Trip (Class 30): Type SB thermal units provide trip characteristics for motor acceleration up to approximately 12 seconds on a full voltage start. The motor must be suitable for extended starting periods.

  • Quick Trip (Class 10): Type FB thermal units are used to protect hermetically sealed, submersible pump motors and other motors that can endure locked-rotor current for a very short time, or motors that have a low ratio of locked-rotor to full-load current.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.