9065CT9701R03/21

Solid-State Overload Relays

The solid-state overload relay (SSOLR) offers some substantial advantages as compared to the traditional NEMA devices, since thermal units are not required:

  • The user does not have to be skilled at the thermal unit selection.

  • Thermal units do not need to be stocked for repair or replacement.

  • Installation time for a starter or separate overload relay can be reduced by 20% to 30%.

The SSOLR, when operated within its operating temperature range, does not require ambient compensation. Only the level of current drawn by the motor affects the tripping of the device.

SSOLRs are typically available as part of a starter or as a separate component. This adds to the flexibility of their application and mounting. Some SSOLRs are designed to retrofit melting alloy or bimetallic devices from the same manufacturer. This flexibility offers you a migration path to the more advanced technology. Backward compatibility can be useful if you decide to standardize on the newer technology, and you wish to upgrade the existing installed base.

Product selection and application are not dramatically different from the traditional melting alloy or bimetallic devices. The mounting and the appearance are also similar to the traditional devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.