9065CT9701R03/21

Table 77

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 77

Motor FLC (A)

Thermal Unit Number

48.0–50.9

FB50.5

51.0–53.7

FB52.5

53.8–57.0

FB55.5

57.1–60.4

FB58.0

60.5–64.0

FB60.0

64.1–71.9

FB63.5

72.0–83.9

FB69.0

84.0–93.1

FB77.0

93.2–104

FB84.0

105–109

FB92.0

110–123

FB105.0

124–133

FB115.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.