9065CT9701R03/21

SoMove™ Software for Configuration

SoMove™ Software Configurator Screen

The TeSys™ T configurator is incorporated in the SoMove™ software application, versions 2.2 and higher.

SoMove software allows configuration, commissioning and maintenance of motor starters protected by a TeSys T controller.

A library containing predefined motor control mode functions is available to:

  • Allow standardization

  • Avoid errors

  • Reduce motor starter setup times

By using logic functions, a custom mode makes it possible to:

  • Easily adapt these predefined motor control mode functions to the specific needs of your applications

  • Create new functions

The defined functions can be saved and used to build your function library for future applications.

To create special functions, a logic editor is incorporated in the configurator and allows a choice of two programming languages:

  • Function block

  • Structured text

Configuration Tools

Description

Composition

Catalog Number

Connection kit for PC serial port for Modbus™ PLC multidrop connection

1 x 3 m length cable with two RJ45 connectors

VW3A8106

One RS232/RS485 converter with one 9-pin female SUB-D connector and one RJ45 connector.

USB serial port adapter for connecting a TeSys T controller to your PC*

1 USB / serial port adapter*

TSXCUSB485

USB serial port cable for connecting a TeSys T controller to your PC

1 USB / serial port cable

TCSMCNAM3M002P

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.