9065CT9701R03/21

NEMA Style Melting Alloy Overload Relays Dimensions

NOTE: These dimensions are for reference only. If you need precise measurements, contact the Customer Care Center at 1-888-778-2733.

NEMA Style Melting Alloy Overload Relays, Dimensions A–H

Type

Dimensions (in.)

Shipping
Weight
(lb)

A

B

C

D

E

F

G

H

SEO5

3.31

0.47

3.97

3.53

2.81

0.22

0.69

1

SEO8

3.31

0.47

3.97

3.5

2.81

0.19

0.69

1.25

SEO12

5.59

0.56

5.75

5.31

4.75

0.28

1.44

3

SEO15

6.97

0.56

5.75

5.31

4.75

0.28

2.13

4

NEMA Style Melting Alloy Overload Relays, Dimensions I–P

Type

Dimensions (in.)

Shipping
Weight
(lb)

I

J

K

L

M

N

O

P

SEO5

2.31

0.5

0.5

0.5

0.84

1

1.38

#10

1

SEO8

2.31

0.5

0.5

0.13

0.84

1

1.38

#10

1.25

SEO12

3.56

0.75

0.56

0.88

1.5

1.75

2

#1/4

3

SEO15

3.56

0.75

0.56

0.88

1.5

1.75

2

#1/4

4

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.