9065CT9701R03/21

Table 147

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 147

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

1.04–1.14

0.93–1.04

B1.30

1.15–1.29

1.05–1.18

B1.45

1.30–1.43

1.19–1.33

B1.67

1.44–1.56

1.34–1.43

B1.88

1.57–1.79

1.44–1.67

B2.10

1.80–2.03

1.68–1.88

B2.40

2.04–2.26

1.89–2.09

B2.65

2.27–2.51

2.10–2.41

B3.00

2.52–3.03

2.42–2.79

B3.30

3.04–3.31

2.80–3.15

B3.70

3.32–3.73

3.16–3.54

B4.15

3.74–4.07

3.55–3.75

B4.85

4.08–4.49

3.76–4.22

B5.50

4.50–4.76

4.23–4.46

B5.25

4.77–5.44

4.47–5.09

B6.90

5.45–6.04

5.10–5.61

B7.70

6.05–6.46

5.62–5.99

B8.20

6.47–7.24

6.00–6.70

B9.10

7.25–8.64

6.71–8.19

B10.20

8.65–9.59

8.20–8.79

B11.5

9.60–10.5

8.80–9.66

B12.8

10.6–11.3

9.67–10.2

B14.0

11.4–12.6

10.3–11.4

B15.5

12.7–13.9

11.5–12.6

B17.5

14.0–14.9

12.7–13.5

B19.5

15.0–16.5

13.6–15.1

B22.0

16.6–18.9

15.2–17.2

B25.0

19.0–22.2

17.3–19.9

B28.0

22.3–24.6

20.0–22.5

B32.0

24.7–28.6

22.6–26.2

B36.0

28.7–32.4

26.3–29.9

B40.0

32.5–37.3

B45.0

37.4–39.5

B50.0

39.6–40.0

B56.0

For Type DPSO42 & DPSO43, 40 A starter, select any of the Thermal Units from above.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.