9065CT9701R03/21

Table 54

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 54

Motor FLC (A)

Thermal Unit Number

2.T.U.

3 T.U.

43.6–45.5

41.1–43.5

CC64.3

45.6–49.6

43.6–46.8

CC68.5

49.7–53.1

46.9–50.0

CC74.6

53.2–57.6

50.1–54.9

CC81.5

57.7–62.4

55.0–57.5

CC87.7

62.5–67.5

57.6–61.8

CC94.0

67.6–71.1

61.9–66.2

CC103.0

71.2–75.9

66.3–72.4

CC112.0

76.0–81.9

72.5–78.1

CC121.0

82.0–84.6

78.2–80.7

CC132.0

84.7–90.7

80.8–86.5

CC143.0

90.8–98.4

86.6–93.9

CC156.0

98.5–105.

94.0–100.

CC167.0

106.–117.

101.–112.

CC180.0

118.–123.

113.–117.

CC196.0

124.–133.

118.–123.

CC208.0

124.–133.

CC219.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.