9065CT9701R03/21

Table 26

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 26

Size 7 Type J

Size 8 Type K

Thermal Unit Number

Current Transformer Ratio

120/5

2000/5

Motor FLC

166.–187.

277.–312.

B1.03

188.–211.

313.–352.

B1.16

212.–232.

353.–388.

B1.30

233.–267.

389.–445.

B1.45

268.–301.

446.–503.

B1.67

302.–336.

504.–561.

B1.88

337.–383.

562.–640.

B2.10

384.–425.

641.–708.

B2.40

426.–466.

709.–777.

B2.65

467.–522.

778.–870.

B3.00

523.–587.

871.–978.

B3.30

588.–656.

979.–1093.

B3.70

657.–764.

1094.–1215.

B4.15

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.