9065CT9701R03/21

Class 9998 Jumper Strap Kits

Jumper Strap Kit Diagram

Jumper strap kits are for use on three-phase manual or magnetic starters with melting alloy overload relays only, where a three-phase starter is used to control a single-phase motor. These kits include two jumper straps, a wiring diagram showing how to wire a three-phase starter to control a single-phase motor, and single-phase (one thermal unit) selection tables.

Class 9998 Melting Alloy Overload Relay Jumper Strap Kits

Class

For Starter

Kit Catalog Number

Size

Type

ALL

00, 0, 1, 2
and M0 & M1

SA, SB, SC, SD and
M & T (Manual)

9998SO31

3,4

SE, SF

9998SO32

5

SG

None Available

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.