9065CT9701R03/21

Table 69

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 69

Motor FLC (A)

Thermal Unit Number

1 or 2.T.U.

3 T.U.

3.46–3.90

3.38–3.65

B4.85

3.91–4.44

3.66–4.07

B5.50

4.45–4.91

4.08–4.36

B6.25

4.92–5.51

4.37–5.19

B6.90

5.52–5.84

5.20–5.59

B7.70

5.85–6.54

5.60–5.98

B8.20

6.55–7.33

5.99–6.78

B9.10

7.34–8.31

6.79–7.91

B10.2

8.32–9.22

7.92–9.12

B11.5

9.23–10.0

9.13–10.0

B12.8

10.1–11.2

10.1–10.7

B14.0

11.3–12.5

10.8–12.0

B15.5

12.6–14.2

12.1–13.5

B17.5

14.3–16.1

13.6–14.6

B19.5

16.2–18.4

14.7–16.7

B22.0

18.5–20.5

16.8–18.9

B25.0

20.6–23.2

19.0–21.6

B28.0

23.3–26.6

21.7–24.1

B32.0

26.7–29.6

24.2–27.6

B36.0

29.7–33.5

27.7–31.2

B40.0

33.6–37.2

31.3–35.5

B45.0

37.3–41.5

35.6–37.8

B50.0

41.6–45.0

37.9–41.5

B56.0

41.6–45.0

B62.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.