9065CT9701R03/21

Thermal Unit Selection on an Approximate Basis—Based on Horsepower and Voltage

Thermal units selected using approximate full-load currents from the table titled Use This Table Only When the Motor Full-Load Current Is Not Known will provide a trip current between 101% and 125% of full-load current for many 4-pole, single speed, normal torque, 60 Hz motors. Since full-load current rating of different makes and types of motors vary widely, these selections might not be suitable.

Thermal units should be selected on the basis of motor nameplate full-load current and service factor. Thermal unit sizes originally selected on an approximate basis should always be rechecked and corrected at the time of installation if required.

How to use the table titled Use This Table Only When the Motor Full-Load Current Is Not Known:

  1. Locate the motor horsepower and voltage.

  2. Determine the approximate full-load current from the table Use This Table Only When the Motor Full-Load Current Is Not Known.

  3. Use the approximate full-load current in place of actual nameplate full-load current and follow the selection procedure in Procedure for Thermal Unit Selection.

NOTE: These currents should not be used for selection of fuses, circuit breakers, or wire sizes. See NEC tables 430-248 through 430-250. For motors rated 208-220 volts, use 230 V column. For motors rated 440 to 550 volts, use 460 and 575 V columns, respectively.

Use This Table Only When the Motor Full-Load Current Is Not Known

Motor
Horsepower

Motor Full-Load Current

Three Ø

Single Ø

200 V

230 V

460 V

575 V

115 V

230 V

   1/6

4.4

2.2

   1/4

5.8

2.9

   1/3

7.2

3.6

   1/2

2.5

2.2

1.1

0.9

9.8

4.9

   3/4

3.7

3.2

1.6

1.3

13.8

6.9

  1

4.8

4.2

2.1

1.7

16

8

    1-1/2

6.9

6.0

3.0

2.4

20

10

  2

7.8

6.8

3.4

2.7

24

12

  3

11.0

9.6

4.8

3.9

34

17

  5

17.5

15.2

7.6

6.1

56

28

    7-1/2

25.3

22

11

9

80

40

 10

32.2

28

14

11

50

 15

48.3

42

21

17

 20

62.1

54

27

22

 25

78.2

68

34

27

 30

92

80

40

32

 40

120

104

52

41

 50

150

130

65

52

 60

177

154

77

62

 75

221

192

96

77

100

285

248

124

99

125

359

312

156

125

150

414

360

180

144

200

552

480

240

192

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.