9065CT9701R03/21

Overview

TeSys™ T Motor Management System Components

TeSys™ T is a motor management system that provides the following:

  • Full motor monitoring, control, and protection when used with short-circuit protection and a contactor

  • Manages most critical processes while reducing downtime and increasing productivity

  • A flexible system that integrates seamlessly into your automation system through five major communication protocols

  • Helps predict what will happen in the process, as it accurately monitors current, voltage, and power over a wide range

  • A green motor management system with unique power monitoring capabilities for better energy management

  • Carries all appropriate and necessary third party certifications

The following sections provide additional information about TeSys T functions.

For detailed information about TeSys T, visit our website at www.schneider-electric.us.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?