9065CT9701R03/21

Table 4

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 4

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

0.32–0.33

0.29–0.30

B0.44

0.34–0.38

0.31–0.35

B0.51

0.39–0.41

0.36–0.37

B0.57

0.42–0.50

0.38–0.45

B0.63

0.51–0.61

0.46–0.54

B0.71

0.62–0.68

0.55–0.61

B0.81

0.69–0.74

0.62–0.66

B0.92

0.75–0.83

0.67–0.74

B1.03

0.84–0.93

0.75–0.83

B1.16

0.94–1.05

0.84–0.93

B1.30

1.06–1.21

0.94–1.07

B1.45

1.22–1.34

1.08–1.19

B1.67

1.35–1.50

1.20–1.33

B1.88

1.51–1.70

1.34–1.51

B2.10

1.71–1.93

1.52–1.70

B2.40

1.94–2.12

1.71–1.87

B2.65

2.13–2.38

1.88–2.10

B3.00

2.39–2.61

2.11–2.29

B3.30

2.62–2.99

2.30–2.63

B3.70

3.00–3.53

2.64–3.09

B4.15

3.54–3.80

3.10–3.32

B4.85

3.81–4.21

3.33–3.67

B5.50

4.22–4.49

3.68–3.91

B6.25

4.50–5.10

3.92–4.43

B6.90

5.11–5.66

4.44–4.91

B7.70

5.67–6.03

4.92–5.23

B8.20

6.04–6.79

5.24–5.88

B9.10

6.80–7.84

5.89–6.77

B10.2

7.85–8.96

6.78–7.90

B11.5

8.97–9.82

7.91–8.44

B12.8

9.83–10.4

8.45–9.05—

B14.0

10.5–11.6

9.06–9.99

B15.5

11.7–12.9

10.0–11.0

B17.5

13.0–13.9

11.1–11.9

B19.5

14.0–15.7

12.0–12.0

B22.0

15.8–18.0

B25.0

Following Selections
for Size M-1 & M-1P Only.

12.0–13.4

B22.0

13.5–15.1

B25.0

17.8–20.1

15.2–17.0

B28.0

20.2–22.2

17.1–18.9

B32.0

22.3–25.3

19.0–21.4

B36.0

25.4–26.0

21.5–24.0

B40.0

24.1–26.0

B45.0

Following Selections
for Size M-1P Only.

25.4–28.4

B40.0

28.5–33.1

B45.0

33.2–36.0

B50.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.