9065CT9701R03/21

Table 16

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 16

Motor FLC (A)

Thermal Unit Number

1.T.U.

2 T.U.

3 T.U.

16.2–17.5

15.1–16.2

14.3–15.4

CC20.9

17.6–18.8

16.3–17.3

15.5–16.4

CC22.8

18.9–20.5

17.4–19.5

16.5–18.5

CC24.6

20.6–22.2

19.6–20.7

18.6–19.6

CC26.3

22.3–23.7

20.8–22.3

19.7–21.1

CC28.8

23.8–25.4

22.4–24.0

21.2–22.7

CC31.0

25.5–27.3

24.1–25.7

22.8–24.4

CC33.3

27.4–29.3

25.8–27.5

24.5–26.1

CC36.4

29.4–31.5

27.6–29.6

26.2–28.1

CC39.6

31.6–33.9

29.7–31.7

28.2–30.0

CC42.7

34.0–36.2

31.8–33.9

30.1–32.1

CC46.6

36.3–39.3

34.0–36.6

32.2–34.7

CC50.1

39.4–42.3

36.7–39.3

34.8–37.3

CC54.5

42.4–45.3

39.4–42.3

37.4–40.1

CC59.4

45.4–48.3

42.4–44.9

40.2–42.6

CC64.3

48.4–52.0

45.0–48.3

42.7–45.8

CC68.5

52.1–54.9

48.4–50.9

45.9–48.3

CC74.6

55.0–59.7

51.0–55.5

48.4–52.6

CC81.5

59.8–65.4

55.6–59.9

52.7–56.8

CC87.7

65.5–69.6

60.0–64.2

56.9–60.9

CC94.0

69.7–74.8

64.3–68.7

61.0–65.1

CC103.0

74.9–79.7

68.8–71.4

65.2–67.7

CC112.0

79.8–83.1

71.5–74.8

67.8–70.9

CC121.0

83.2–86.0

74.9–78.0

71.0–73.9

CC132.0

78.1–80.7

74.0–76.5

CC143.0

80.8–86.0

76.6–80.2

CC156.0

80.3–83.1

CC167.0

83.2–86.0

CC180.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.