9065CT9701R03/21

Table 1

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 1

Motor FLC (A)

Thermal Unit Number

1 T.U

3 T.U

0.33–0.36

0.29–0.32

B0.44

0.37–0.40

0.33–0.36

B0.51

0.41–0.45

0.37–0.39

B0.57

0.46–0.52

0.40–0.47

B0.63

0.53–0.59

0.48–0.56

B0.71

0.60–0.66

0.57–0.63

B0.81

0.67–0.73

0.64–0.69

B0.92

0.74–0.81

0.70–0.77

B1.03

0.82–0.91

0.78–0.86

B1.16

0.92–1.02

0.87–0.96

B1.30

1.03–1.14

0.97–1.11

B1.45

1.15–1.29

1.12–1.23

B1.67

1.20–1.42

1.24–1.37

B1.88

1.43–1.64

1.38–1.55

B2.10

1.65–1.80

1.56–1.75

B2.40

1.81–2.10

1.76–1.92

B2.65

2.11–2.30

1.93–2.16

B3.00

2.31–2.61

2.17–2.50

B3.30

2.62–2.99

2.51–2.81

B3.70

3.00–3.37

2.82–3.16

B4.15

3.38–3.94

3.17–3.40

B4.85

3.95–4.24

3.41–3.76

B5.50

4.25–4.54

3.77–4.00

B6.25

4.55–5.29

4.01–4.68

B6.90

5.30–5.73

4.69–5.18

B7.70

5.74–6.35

5.19–5.51

B8.20

6.36–7.08

5.52–6.19

B9.10

7.09–7.83

6.20–7.12

B10.2

7.84–8.47

7.13–8.15

B11.5

8.48–9.83

8.16–8.60

B12.8

9.84–10.5

8.61–9.21

B14.0

10.6–11.4

9.22–10.1

B15.5

11.5–12.8

10.2–11.2

B17.5

12.9–13.9

11.3–12.0

B19.5

14.0–16.1

B22.0

16.2–18.0

B25.0

Following Selections
for Size M-1 & M-1P Only.

11.3–12.1

B19.5

12.2–13.6

B22.0

16.2–17.6

13.7–15.3

B25.0

17.7–20.6

15.4–17.3

B28.0

20.7–23.1

17.4–19.1

B32.0

23.2–26.0

19.2–21.7

B36.0

21.8–24.2

B40.0

24.3–26.0

B45.0

Following Selections
for Size M-1P Only

23.2–27.1

B36.0

27.2–29.2

B40.0

29.3–33.0

B45.0

33.1–36.0

B50.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.