9065CT9701R03/21

Table 105

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 105

Motor FLC (A)

Thermal Unit Number

105–112

CC74.6

113–122

CC81.5

123–131

CC87.7

132–142

CC94.0

143–153

CC103.0

154–157

CC112.0

158–169

CC121.0

170–181

CC132.0

182–195

CC143.0

196–209

CC156.0

210–227

CC167.0

228–247

CC180.0

248–266

CC196.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.