9065CT9701R03/21

Lug-Lug and Lug-Extender Kits

A Class 9999 LL0 Lug-Lug Kit can be field installed on separately mounted overload relays. The standard Size 00B, 00C, 0, and 1 Class 9065 Type SS and SF overload relays are supplied without lugs. A Class 9999 LB0 Lug-Extender Kit is designed for Size 00B, 00C, 0, and 1 Retrofit Starter Applications. This kit allows the lugs to be in the same location as the Class 9065 melting alloy overload relay, eliminating the need for additional wire length.

Lug-Lug and Lug-Extender Kits

For Use With

Parts Kit
Description

Catalog Number

Catalog Number

NEMA Size*

9065SF

00B, 00C, 0, and 1

Lug-Lug Kit for separate mounting

9999LL0

9065SF

00B, 00C, 0, and 1

Lug-Extender Kit for retrofitting existing NEMA Type S starters

9999LB0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.