9065CT9701R03/21

Table 56

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 56

Motor FLC (A)

Thermal Unit Number

1 or 2.T.U.

3 T.U.

3.29–3.74

3.18–3.40

B4.85

3.75–4.23

3.41–3.76

B5.50

4.24–4.68

3.77–4.00

B6.25

4.69–5.22

4.01–4.57

B6.90

5.23–5.67

4.58–5.03

B7.70

5.68–6.13

5.04–5.32

B8.20

6.14–6.91

5.33–5.97

B9.10

6.92–7.70

5.98–6.88

B10.2

7.71–8.56

6.89–7.82

B11.5

8.57–9.39

7.83–8.47

B12.8

9.40–10.4

8.48–9.15

B14.0

10.5–11.6

9.16–10.1

B15.5

11.7–12.9

10.2–11.2

B17.5

13.0–14.6

11.3–12.0

B19.5

14.7–16.5

12.1–13.6

B22.0

16.6–18.5

13.7–15.2

B25.0

18.6–21.0

15.3–17.1

B28.0

21.1–23.6

17.2–19.0

B32.0

23.7–26.3

19.1–21.5

B36.0

26.4–29.3

21.6–24.1

B40.0

29.4–35.1

24.2–27.0

B45.0

35.2–36.1

27.1–28.7

B50.0

36.2–39.1

28.8–30.4

B56.0

39.2–41.5

30.5–32.2

B62.0

41.6–45.0

32.3–35.4

B70.0

35.5–38.2

B79.0

38.3–45.0

B88.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.