9065CT9701R03/21

Motor Failure and Protection

Motor failure can result from electrical or mechanical factors. A study commissioned by the Electrical Research Associates (ERA) of the United Kingdom in 1986 indicated that the most common causes of motor failure are:

  1. Overcurrent: 30%

  2. Contamination: 18%

  3. Single Phasing: 15%

  4. Bearing Failure: 12%

  5. Aging (natural wear): 10%

  6. Rotor Fault: 5%

  7. Miscellaneous: 7%

Failure modes 1, 3 and 7 are attributable to electrical issues. Failure modes 2, 4, 5 and 6 are the result of mechanical (and some manufacturing) issues.

Historically, motor protection provided with the controller was only able to address the electrical causes of motor failure. These electrical issues account for at least 45% of the most common causes of motor failure.

Motor branch circuits are protected against short-circuits (instantaneous overload currents) and steady-state or low-level, sustained overloads. In the U.S., this protection is provided by the short-circuit protective device (SCPD) and the motor overload relay, when they are applied according to the National Electrical Code® (NEC®).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.