9065CT9701R03/21

Class 9999 Isolated Alarm Contacts

Type SO4

Isolated overload relay alarm contacts are available factory-installed or in kit form for field installation in NEMA Size 00–6 Type S* starters that are factory installed with a Class 9065 Type SE melting alloy overload relay. NEMA Size 7 Type S devices use a solid­state overload relay which has isolated alarm contacts as an optional feature. See the table Isolated Auxiliary Contacts for Motor Logic Overload Relays. The alarm contacts allow the starter to be used in applications that require isolated contacts, such as inputs to a computer.

Class 9999 Types SO4 and SO5 modules are interchangeable with the standard module (Class 9998 Type SO1) and can be installed on starters already in service. The case is made of clear plastic (polycarbonate) to allow for visual inspection of contacts.

Class 9999 Contact Unit for Melting Alloy Overload Relays

Magnetic Starter

Parts Kit Description

Catalog Number

NEMA
Size

Type

00–6 *

SA–SH

N.O. Isolated Alarm Contact Plus
Standard N.C. Overload Contact

9999SO4

N.C. Isolated Alarm Contact Plus
Standard N.C. Overload Contact

9999SO5

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.