9065CT9701R03/21

Remote Reset Module

The Remote Reset Module can be field-installed on solid-state overload relays. This module will allow the overload relay to be reset from a remote location.

Remote Reset Module

For Use With

Parts Kit Description

Catalog Number

Class & Type

NEMA Size*

8536 SA–SJ

00B through 7

Remote Reset Module

9999RR04*

9065 SF, ST

00B through 7

8536 SE–SF

3 and 4

Top Mounting Bracket

9999RB34* *

9065 SF, ST

3 and 4

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.