9065CT9701R03/21

Table 61

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 61

Motor FLC (A)

Thermal Unit Number

2 T.U.

3 T.U.

46.8–50.0

45.3–48.2

CC64.3

50.1–54.2

48.3–52.4

CC68.5

54.3–58.3

52.5–56.4

CC74.6

58.4–63.6

56.5–61.2

CC81.5

63.7–68.5

61.3–66.1

CC87.7

68.6–74.0

66.2–71.4

CC94.0

74.1–79.8

71.5–77.0

CC103.0

79.9–83.0

77.1–79.0

CC112.0

83.1–88.9

79.1–84.7

CC121.0

89.0–95.6

84.8–91.1

CC132.0

95.7–102.

91.2–98.1

CC143.0

103.–109.

98.2–104.

CC156.0

110.–119.

105.–113.

CC167.0

120.–133.

114.–123.

CC180.0

124.–133.

CC196.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.