9065CT9701R03/21

Table 18

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 18

Motor FLC (A)

Thermal Unit Number

1.T.U.

2 T.U.

3 T.U.

15.5–16.4

14.4–15.3

13.6–14.5

CC20.9

16.5–17.6

15.4–16.4

14.6–15.5

CC22.8

17.7–19.1

16.5–18.4

15.6–17.4

CC24.6

19.2–20.4

18.5–19.6

17.5–18.5

CC26.3

20.5–22.1

19.7–21.0

18.6–19.9

CC28.8

22.2–23.4

21.1–22.7

20.0–21.5

CC31.0

23.5–25.6

22.8–24.2

21.6–22.9

CC33.3

25.7–27.3

24.3–25.9

23.0–24.5

CC36.4

27.4–29.4

26.0–27.8

24.6–26.3

CC39.6

29.5–31.5

27.9–29.8

26.4–28.2

CC42.7

31.6–33.7

29.9–31.7

28.3–30.0

CC46.6

33.8–36.5

31.8–34.2

30.1–32.3

CC50.1

36.6–39.1

34.3–36.9

32.4–34.9

CC54.5

39.2–41.7

37.0–39.8

35.0–37.6

CC59.4

41.8–44.8

39.9–42.3

37.7–40.0

CC64.3

44.9–48.0

42.4–45.3

40.1–42.8

CC68.5

48.1–50.7

45.4–47.9

42.9–45.3

CC74.6

50.8–54.9

48.0–51.9

45.4–49.1

CC81.5

55.0–59.9

52.0–56.5

49.2–53.4

CC87.7

60.0–63.3

56.6–60.7

53.5–57.4

CC94.0

63.4–67.2

60.8–64.8

57.5–61.3

CC103.0

67.3–72.4

64.9–67.1

61.4–63.5

CC112.0

72.5–74.9

67.2–70.1

63.6–66.3

CC121.0

75.0–77.4

70.2–72.9

66.4–69.0

CC132.0

77.5–80.7

73.0–74.9

69.1–70.9

CC143.0

80.8–83.1

75.0–77.9

71.0–73.7

CC156.0

83.2–86.0

78.0–80.9

73.8–76.5

CC167.0

81.0–82.9

76.6–78.4

CC180.0

83.0–86.0

78.5–86.0

CC196.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.