9065CT9701R03/21

Protection Functions

  • Thermal overload

  • Phase imbalance and phase failure

  • Thermal motor protection via PTC probes

  • Phase reversal

  • Ground fault detection

  • Long starting times and motor stalling

  • Automatic load shedding and restarting

  • Load fluctuations (current, voltage, power)

  • Variations of Cos j (power factor)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.