9065CT9701R03/21

Table 146

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 146

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

3.90–4.22

3.60–3.89

B5.50

4.23–4.49

3.90–4.15

B6.25

4.50–5.14

4.16–4.76

B6.90

5.15–5.78

4.77–5.30

B7.70

5.79–6.23

5.31–5.70

B8.20

6.24–7.03

5.71–6.46

B9.10

7.04–8.23

6.47–7.65

B10.2

8.24–9.31

7.66–8.55

B11.5

9.32–10.1

8.56–9.36

B12.8

10.2–10.7

9.37–9.9

B14.0

10.8–11.9

10.0–10.9

B15.5

12.0–13.1

11.0–12.0

B17.5

13.2–13.9

12.1–12.8

B19.5

14.0–15.9

12.9–14.2

B22.0

16.0–18.0

14.3–16.0

B25.0

18.1–20.8

16.1–18.5

B28.0

20.9–23.1

18.6–21.2

B32.0

23.2–26.9

21.3–24.9

B36.0

27.0–31.4

25.0–28.0

B40.0

31.5–36.0

28.1–31.7

B45.0

36.1–38.8

31.8–34.6

B50.0

38.9–41.7

34.7–37.4

B56.0

41.8–46.3

37.5–40.0

B62.0

46.4–50.0

40.1–46.4

B70.0

46.5–50.0

B79.0

For Type DPSG52 & DPSG53, 50 A starter, select any of the Thermal Units from above.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.